Other Parts Discussed in Thread: AWR1642
Hi,
I have an IWR1642 boost evm and I want to try the Vital Signs Measurement demo but I see that in the new industrial toolbox v2.0.0 the demo is for xwr1443.
Looking in the automotive toolbox v1.0.0.0 I found the demo for AWR1642 so I have two question:
1) can I run the Vital Signs Measurement demo for AWR1642 on a IWR1642 boost evm?
2) if the above response is true I have another problem. My evm was reworked to route the data cfg COM out of J6 connector instead of USB connector (remove 0ohm from R128/R129 and soldered 0ohm on R166/R169). So to connect to the evm I use the data COM over usb and a 3.3v serial-to-usb converted for cfg COM.
When I run on the host the gui "mmwave_automotive_toolbox_1_0_0\labs\lab0001-driver-vital-signs\vitalSigns_host\gui\gui_exe\VitalSignsRadar_Demo.exe" It will autodetect the COM port and I can't change it's value to match the one of my serial to usb converter. How can I change the COM port in gui (clicking on "Setting" menu I cant select other COM port)? Looking in "mmwave_automotive_toolbox_1_0_0\labs\lab0001-driver-vital-signs\vitalSigns_host\gui\gui_source" I see there are the sources of the gui and in dialogsettings.cpp there is the COM configuration. If I modify this source to match my COM port name then how can I rebuild the GUI? I did not find documentation on how to do it
Regards,
Luca