This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDC1000-GASEVM: TDC1000-GASEVM

Part Number: TDC1000-GASEVM

I have a question regarding the Ultrasonic Analog Front End and Time-to-Digital Converter Evaluation Module (TDC1000-GASEVM and TDC1000-BSTEVM), I just want to know the operation current for this evaluation module.

 

Thanks.

  • Hi Mohammed,

    Without modifying the board to directly test the current from the USB port, the current draw of the MSP430 is the largest portion of the power consumption. I see about 13mA being drawn total for all the major components even when measuring.

    Regards,