Hi team,
The customer is using IW1642BOOST. The customer refers to 4. 2. How to flash an image onto xWR14xx/xWR16xx EVM
of the MMWAVE SDK 1.1 User Guide, when he uses the demo mode, then uses the mmWave Demo Visualizer,
there is the data on the mmWave Demo Visualizer. This is fine in the demo mode.
But when he uses the CCS development mode, and download the xwr16xx_ccsdebug.bin file to the IW1642BOOST,
there is not any data in the mmWave Demo Visualizer when he uses the mmWave Demo Visualizer.
So, if the customer uses the CCS development mode, how should he do correctly?
Best Wishes,
Mickey Zhang
Asia Customer Support Center
Texas Instruments