This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1642BOOST: Reading the UART part without USB

Part Number: IWR1642BOOST
Other Parts Discussed in Thread: IWR1642

Hi,

I have brought a IWR1642 BOOST EVM for vehicle detection. I tried the mmWave Visualiser and was able to detect the desired objects in the X-Y plot and the doppler plot. 

I would like to now get the data of the detected objects using a microcontroller. I know the EVM has a UART port but i see no data coming out of it ( used an osciloscope to check) even when the Visualiser is running. 

What is the best way to interface with a microcontroller which has no USB port to read the data from.