Other Parts Discussed in Thread: AWR1642
Hello, I am HJ.
I am looking for awr 1642 chip detection capability.
The box below is a specification for a chip that I understand.
is it right or wrong, I don't know. I want to know official awr 1642 detection capability.
|
Far Range |
Near Range |
§Max Range
|
80m |
20m |
§Range Resolution
|
35cm |
4.3cm |
§Max Velocity
|
90km/h |
36km/h |
§Velocity Resolution
|
1kmph |
1kmph |
§RCS
|
1 m2 |
0.1m2 |
§Horizontal FOV
|
120 deg. |
120 deg. |