Other Parts Discussed in Thread: AWR1642
Hello I'm HJ
▪ How to set AWR 1642 USRR
1. How to set AWR 1642 USRR in Visualizer?
2. When set to Best Range Resolution in Visualizer, Maximum Unambiguous Range is 10.8m maximum, is this USRR mode?
3. If not, how? If it is set to Config, request Config file or request to provide configuration parameter
4. Best Range Resolution was measured and considered in USRR mode. Measuring only 120 degrees. The information sheet says 160 degrees. How can you measure up to 160 degrees?
▪ How to set AWR 1642 SRR
1. How to set AWR 1642 SRR in Visualizer?
2. When set to Best Range in Visualizer, Maximum Unambiguous Range is 50m maximum, is this SRR mode?
3. If not, how? If it is set to Config, request Config file or request to provide configuration parameter
4. When setting the best range in Visualizer, maximum unambiguous range is set to 50m. In the brochure, a detection distance of 100m was shown in srr mode. how do you test with 100m set?