Other Parts Discussed in Thread: TPS7A8101
Hi champion,
My customer ran mmwdemo in SDK 1.1.0.2 on their 1642 board, but find demo failed on below error. Could you help to check what is the meaning for error code -13021?
Thank you,
Adam
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Cesar,
Just got from customer, they replaced the LP87524, TPS7A8101, TPS7A8801 with the PMIC from other vendors (which output 1.8/1.3/1.2/3.3V). Is there any powering up sequence requirement which could cause this problem?
Thank you,
Adam
Adam,
Are they running the pre-built binaries along with one of the provided (i.e. unaltered) profile configs? If they are, then yes, it may be a hardware issue. If not, then they should try running with the provided binaries and configs.
-dave
Hi Dave,
Thanks for your reply. The issue has been resolved. The rootcause is customer was using a low pull-up resistor on SOP pin which cause the chip went into Debug mode.
Thank you,
Adam