Dear Support,
I was wanting to ask if you could help me with the following questions:
In the following post you explained how to calculate the voltage level at the receiver ADC input for a given RF power at the input to the receiver:
So full scale at the I/Q ADC input is 1 Vpeak which is +10dBm at the input to the I/Q ADC (assuming 50ohm input impedance) which for a receive gain of 48dB would correspond to -38dBm CW (sinusoidal) at the input to the receiver. So I/Q ADC level (dBFs) = RX input level (dBm) + RX gain (dB) - 10dBm.
However on the datasheet in Figure 5-1 the receiver input in-band P1dB is ~-47dBm at a receiver gain of 48dB.
Q1. Why is the receiver in-band P1dB 9dB lower than the ADC full-scale receiver input level of -38dBm. Can you let me know what element in the receiver chain is causing this compression before the ADC has reached full-scale?
Q2. Can you also confirm that the equation above for calculating the I/Q ADC level (in dBFs) from the RX input power is correct?
I appreciate your help with this.
Yours faithfully,
Jonathan Jones