Team,
Please help verify the appropriate set up:
I’m using the UART interface at 3.3V, and I want to make sure I have all the connections correct per TI’s recommendations:
- TXD connected to master microcontroller’s RX with internal weak pull-up
- RXD pulled up to 3.3V with 100kΩ resistor
- SCLK pulled low with 100kΩ resistor
- IO, TEST, and DECPL pins left unconnected. Or do I need to pull TEST low to ensure 3.3V functionality?
Please help confirm or correct the above pin connection descriptions if possible.
Thanks
Viktorija