Other Parts Discussed in Thread: UNIFLASH,
Hi,
I am using the most recent version of the radar studio, mmwave_dfp and all the firmware files. I am trying to flash the onboard serial flash with the rf_eval firmware files and I am not successful with Radar Studio or the most recent Uniflash tool. I am following all the instructions including the right jumpers on the AWR1243BOOST to set the device in flash mode. I make sure that I power cycle.
I choose the COM Port on my computer which belongs to XDS110 Class Application User UART but both the tools cannot find the port.
When I remove the jumper to go back to development mode , and power cycle the chip, then I can connect on the same port in development mode. I made sure that in the Uniflash tool, the session points to the right COM port.
Similarly in Radar Studio, I made sure that I choose SOP mode for flashing, and not click set. Then I also made sure that right COM port is chose in RS232 Connectivity without pressing the Connect button. When I click the Flash Program button, a window opens up but goes away quickly and has the port opening error messages.
Thank you for the help !
Regards,
RJ