Other Parts Discussed in Thread: IWR1642
Hi,
I am intended to use the IWR1642 radar for short-range (within 1 meter) human detection. In addition, I hope to lower down the power of radar due to safety concern (as the distance to the human head may be only 10 cm). However, I noticed that the Rx gain cannot be lower than 24dB as indicated in the SDK. And I cannot make the maximum detection range lower than 6.4 meters.
Any suggestion? If the IWR1642 radar is not suitable for this application, is there any other option?
Regards,
James