This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1642: mmwave demo not works in best velocity in best velocity resolution mode if we choose number of rx=2 or 1 (SDK version-1.1)

Part Number: AWR1642


Hi,

when we choose number of rx=2 or rx=1 in best velocity resolution demo visualizer is not working.Checked in ccs and program won't run after passing below config file  and we are not getting any error message also. Please find the below configuration which we used.Is there any specific reason for this behaviour?

flushCfg
dfeDataOutputMode 1
channelCfg 2 1 0
adcCfg 2 1
adcbufCfg -1 0 0 1 0
profileCfg 0 77 3888 7 18.24 0 0 27.412 1 64 6249 0 0 30
chirpCfg 0 0 0 0 0 0 0 1
chirpCfg 1 1 0 0 0 0 0 0
frameCfg 0 0 128 0 1000 1 0
guiMonitor -1 1 1 0 0 1 1
cfarCfg -1 0 0 8 4 4 0 640
cfarCfg -1 1 0 8 4 4 0 640
peakGrouping -1 1 1 1 1 63
multiObjBeamForming -1 1 0.5
clutterRemoval -1 0
calibDcRangeSig -1 0 -5 8 256
extendedMaxVelocity -1 0
compRangeBiasAndRxChanPhase 0.0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0
measureRangeBiasAndRxChanPhase 0 1.5 0.2
sensorStart

Thanks,

Preetham