This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE4300EVM-PDK: Where to connect the wires at impedance simulation block

Part Number: AFE4300EVM-PDK


Hello team,

Please see below question from the customer:

I am trying to follow the development user manual for the evm (http://www.ti.com/lit/ug/sbau201a/sbau201a.pdf). There is this following section:

 

 

But I am not sure where should I connect the wires to at the impedance simulate block. There are jumper locations at J39, J41 to J45, some of them are left out open and some are populated with 0 Ohm. Which of these jumpers actually is driven by the SW3 third position?