Other Parts Discussed in Thread: AWR1642
Hello,
Please let me know the cause and solution of the false detection with AWR1642BOOST.
In case the reflector is located at 1.5m far from AWR1642BOOST, the false detection is at the maximum detectable distance - 1.5m.
The maximum detectable distance is calculated by the following formula using profileCfg parameters.
The maximum detectable distance = (sampling rate) x c / 2 / slope = (5583e+3)*(3e+8)/2/(21.53e+12)=38.9m
The red circle in the following figure shows the false detection.
The false detection point is about 37.4m (38.9m - 1.5m).
The conditions are following.
-AWR1642BOOST is used for the evaluation.
-The firmware is pre-build binary in the mmWave SDK (version is v01.00.00.05).
-Demo visualizer is used for the evaluation and the version is v1.2.0.
-The configure file is attached.
Best Regards,
Nomo