This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/AWR1642: CAN-bus will crash when computer suddenly stop connect.

Part Number: AWR1642

Tool/software: TI-RTOS

I use the CAN-bus to transmit data of mmwave.

First, open the CAN-bus on computer and send CLI command to AWR1642.

AWR1642 can successfully transmit data.

After the computer suddenly  close the CAN-bus, the computer restarts CAN-bus.

It can't receive any data from AWR1642. And computer still can send CLI command to AWR1642. It will receive Done or Error -1.

Is there any method avoid CAN-bus crash in this case?

Regards,

Jui Yang