This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1443: Altium importable file for IWR1443 reference design

Part Number: IWR1443


Hi Support,

Request to IWR1443BOOST board PCB design files in Altium importable format.

http://www.ti.com/tool/iwr1443boost

Details for conversion can be found at the following link:

http://www.altium.com/documentation/18.0/display/ADES/((Allegro+Import))_AD

Since I don't have a licensed version of Allegro, it will be helpful if you can provide required ASCII file.

Is there a document which can be used as the reference for antenna design for IWR1442?

Thanks in advance.

Best Regards,

Satyan Raj

  • Hello,

    We have tried the Cadence to Altium conversion, since this didn;t work for us.  An Altium 1443 database is planned to be constructed in the second quarter.

    The xWR1642 ES2 data package that will be released in the next 45 days,   Many of the parts are the same, except for the U2 mmwave sensor, the HD60 connector

    has different connections, the antenna DXF file is different.  

    There is no direct 1443 Altium conversion yet.

    Regards,

    Joe Quintal

  • Thanks for the update