This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDC1000-C2000EVM: if we can use signal generator to deliver 1MHz to Rx1 pin, then to measure to measure 1us period? How to set up register?

Part Number: TDC1000-C2000EVM
Other Parts Discussed in Thread: TDC1000

Hi Sir 

We have some EVB application question as attached file.

May you pls help advise?

                                             Bogey

TDC.docx

  • Hi Bogey,

    From the document attached, the Error message states the correct action to take to fix the problem with writing the registers. The firmware for the MSP430 on the EVM needs to be updated. This can be done through the GUI on the Debug tab. The full instructions for updating the GUI are included in the user's guide: www.ti.com/.../sniu021a.pdf

    I'm curious about the application for this. Is the final goal to eventually use ultrasonic transducers to measure level or concentration? If so, the TDC1000 is a good fit. However, if the application is to simply measure the period of a digital input signal I do not recommend the TDC1000. That could be done with the C2000 alone.

    Regards,