This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR6047: Water Flow meter values (in LPH) are less than actual flow.

Part Number: MSP430FR6047


Hi,

I am working on MSP430FR6047 base water flow meter. I am using AudioWell 25mm brass flow tube.

I ran  "USSLib_GUI_Demo" and loaded default USS parameters from GUI application.

I found that the reading are much less than actual flow.

Then I found valid meter constant range is 0 to 22742000 as set it to MAX possible i.e. (22742000)

But still I am getting reading 10 times less than actual. 

and if I increase meter constant above the range to match reading with actual flow then it is causing higher variation at low flow.

also at zero flow , reading fluctuates in +/- 10 LPH