Other Parts Discussed in Thread: PGA460
Dear TI,
For my ultrasonic application it is required that I filter out all readings that are 5 cm from the ground. this is in order to make AGV drive without stopping for small objects, for which another mechanism is used. how do i create a blind zone in which no objects are seen. in the past we used a pepperl fuchs sensor which was able to manipulate the beam characteristics. is it possible to do this with the PGA460 or do I need a special transducer.
I've done some testing with EVM and i cannot differentiate between the objects when they have the same amplitude. also my sensor height is fixed so I cannot simply place it higher.
Kind regards,
Glenn