Other Parts Discussed in Thread: MMWAVE-SDK
Tool/software: Code Composer Studio
CCS is V8
SDK version is mmwave_sdk_01_01_00_02
Want to build two project--mmw_dss_16xx,mmw_mss_16xx which from Millimeter Wave Demo.
However,it can't well done.Here is the Problem.
Hope someone could help me. The following is the building messages of DSS. The message also happens to MSS project.