This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP112: TMP112 temp issue

Part Number: TMP112


hi  

our customer meet one issue when test Tmp112, it will show one abnormal high temp( such as 173°C), or abnormal low temp(ext:0.1°c.

they are all in the log on list, pls refer below log information:

could you tell us, why was happen it?


  • Hi Lina,

    Please share oscilloscope pictures of your I2C Bus. If possible, capture the abnormal read with the oscilloscope. If you can't capture the abnormal read, I'll still need to see oscilloscope picture of normal operation to provide further support.

    Thanks,
    Ren