This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1243: The maximum capture duration in TSW1400

Part Number: AWR1243


Hi,

My customer test with the AWR1243+TSW1400 to capture raw data, and they find the maximum capture duration is 10s once. In my opinion the maximum capture size and duration should be restricted by the DDR size in TSW1400, right? If yes i cannot understand why the maximum duration is 10s, would u pls help confirm?

And if customer want to increase the capture duration, is it possible to replace with one big size DDR? 

Thanks & BR,

Andy

  • Hi Andy,

    10s is the supported maximum capture duration.

    We are working to release this month a Data capture card that would be able to stream the data through ethernet to a PC. I think this is the solution that your customer needs.

    Thank you
    Cesar