This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1443BOOST: Using two transmit channels

Part Number: AWR1443BOOST

Hello,

I'm using the capture demo to collect the raw ADC data and trying to use two transmit channels.

1. Do the two transmit channels transmit signals at the same time or channel 1 transmits a chirp first and then channel 2 transmits a chirp?

2. Can the two transmit channels transmit different chirps?

3. What is the order of the stored received signal data if I use two transmit channels?

Thanks,

Yun