We are using multiple AFE4490 EVM boards. I have a Lenovo ThinkPad running Windows 10. For some of the modules, the AFE GUI software recognizes the board and works well, but for others which are exactly the same, it seems that the software doesn't recognize it. The devices are all recognized in device manager as a COM port and correct driver is updated, but when we open the AFE GUI software, it doesn't recognize some of the boards. It gives me the following error "An error occured while communicating with the device. Press Continue to Simulate Communication. Press Stop & Close to Exit". All of the boards work on a colleague's laptop, which indicates that the boards are functioning properly. What could be the issue?