Tool/software: WEBENCH® Design Tools
Hi, I am making a device which is measure human feet temperature by puting LMT70 in the insole shoes. However, i am using Thin Flexible Circuit Board Materials with a low modulus polyimide with 40 LMT70 on the top of the PCB. I have tried my circuit and the sensors worked well.
1- I have read in the data sheet that the measurement for LMT70 should be from the button of the sensors is that the best option?
2- What material should I use to make the best connectivity between the LMT70 and human skin in order that i am using Flexible Circuit polyimide ?
3- can I put any material on the top of LMT70 which will not effect the temperature measurement in order that the sensors will be in insole of shoe?
Best regards