Other Parts Discussed in Thread: IWR1443,
We are evaluating the IWR1443 for use in a drone to enhance obstacle detection and mapping, especially around glass obstacles like windows.
I got the IWR1443BOOST to work with ROS and was getting 3D point cloud data in Rviz. However, while the visualization captured obstacles like people and chairs, I did not see any indication that walls (dry wall) or windows were being detected. My assumption is that the walls are being detected, but are being filtered out. For our application, we would ideally see a point cloud representation of flat wall surfaces that could be used to build a map of a room, like what you get with a LIDAR.
My questions are:
1. Can the IWR1443 be used to generate a point cloud showing walls like I am describing?
2. Is this something that can be done with Out-of-Box Demo firmware or do I need to dig a bit deeper before I can really evaluate this sensor?
Thank you.