This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1642: Our 2 AWR1642s have both stopped being able to calculate doppler speed.

Part Number: AWR1642

We have been working with 2 AWR1642 Radars, and they both worked... Then at some point both of the Radars stopped sending a correct doppler reading. For any and all points the doppler value is in-between -1 to 1 m/s, but it just seems kind of random.   To Isolate the problem we tried both the radars with multiple computers, and did not use any of our code, and simply just used the stock firmware, and read the data with the web based, Ti mmwave visualizer,   and in all cases we still observe that the doppler reading is not making any sense. 

So this makes us believe it is a hardware problem with the radar.  However, it seems odd because it happened to both of our AWR1642s

Does anyone have any ideas about this?

Thanks