This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1443BOOST: EVM stack up information

Part Number: IWR1443BOOST

Hi,

I have a customer who is interested in mmWave and started to looking into TI documents.
They found PCB stack-up (IWR1443BOOST_Rev-A-Stackup.pdf) and have below questions.

http://www.ti.com/general/docs/lit/getliterature.tsp?baseLiteratureNumber=sprr253&fileType=zip

In upper table:
Q1) There are two thicknesses(Base and Processed) for each layer.
What does they mean?
Q2) Why IteqIT layer is double-deck ?
Q3) What does the “Description” mean, name of materials ?

In lower table:
Q1) Please explain what does this table mean. This is not easily understandable.

Thanks and regards,
KoT

  • Hello,

    I have answers for some of these questions.

    Utilizing the IWR1443BOOST_Rev-A Stackup.pdf 

    Q1) the Base is the initial thickness, before the board is pressed together.

           the Processed thickness is after the board is pressed

    Q2) Prepreg layer - see discussion "www.pcbcart.com/.../layer-stackup.html

    the resin and weave of the resin provide the mechanism to combine the layers.

    L1 (top copper), 4mil core, and L2 (GND) are combined with the other layers.  There is a balancing L6 (bottom) 4mil core, L5 (GND) on the PCB.   

    The two internal Layers L3, L4 are separated around the core, and there are two prepreg - resin / adhesive layers.

    The double thickness depends on the PCB construction.  Different PCB houses have specific mechanical rules that can vary the processed thickness.

    Q3) Description - this is the material that the PCB board layers are made of.  Each of them has a datasheet, and is selected for a specific purpose:

         1) RF surface layer, core, and GND layer - Rogers material 4835 4mil core, Lo Pro

         2) Iteq 180A top and bottom prepreg pairs - this has resin and weave to combine the Rogers, Copper planes, Core 28mil.

             thickness and Iteq 180A - this is PCB design house thickness.

         3) Layer 3 Copper to Core to Layer 4 Copper has a different impedance from the Rogers 4835 L1, L2, and L5 Cu to 4mil ITEQ108A to L6 Cu.

         4) double layer Prepreg - provides more bonding adhesive than a single layer

    Q4) The table at the bottom discusses for critical signals on the schematic RF Tx, RF Rx, and LVDS differential pairs.   

    Regards,

    Joe Quintal