This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1243: How to determine the spectral power

Part Number: AWR1243


Hi mmWave Champs,

Once you post-process the raw ADC data and you apply the FFT analysis, there should be a correction factor that need to be used to represent the spectral power in terms of dBFS or dBm. Please advise how to retrieve power figures from FFT results.

Thanks,
Peter. 

  • Hello Peter,
    Typically when a FFT is done in matlab the signal amplitude gets multiplied by the number of points of the FFT. If you do a N point FFT the amplitude is got by dividing the FFT peak by N.
    Once the amplitude is got the dBFs is got by comparing it with the ADC full scale amplitude. For a 12bit ADC mode , for example, the full scale is +-2^11 , ie +-2048. So if the amplitude got is 1024 , for example, the dBFs would be 10*log(1024/2048), ie -3dBFs.

    Regards,
    Vivek