This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1443: Is it possible to open individual 1 tx antenna by configuring channelCfg ?

Part Number: IWR1443


I tried to open tx antenna by following config:

channelCfg 4 2 0 and channelCfg 4 4 0, all failed.

I found the tx antenna only available for number 1, 3, 5,7, but not available for 2, 4, is this the restriction of hardware?

  • Hi,

    The  tx antenna channel can be set to any channel, 1 2 3 4 5 6 7 are available for this value.

    Which SDK you are using? The latest one is SDK1.2

    Also, when you change the TX channel, you should change the chirp config too. Here's an example.

    sensorStop
    flushCfg
    dfeDataOutputMode 1
    channelCfg 15 4 0
    adcCfg 2 1
    adcbufCfg 0 1 0 1
    profileCfg 0 77 52 7 40 0 0 100 1 128 4000 0 0 30
    chirpCfg 0 0 0 0 0 0 0 4
    frameCfg 0 0 32 0 400 1 0
    guiMonitor 1 1 1 1 0 1
    cfarCfg 0 2 8 4 3 0 2000
    peakGrouping 1 1 1 1 112
    multiObjBeamForming 1 0.5
    calibDcRangeSig 0 -5 8 256
    clutterRemoval 0
    compRangeBiasAndRxChanPhase 0.0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0
    measureRangeBiasAndRxChanPhase 0 1.5 0.2
    sensorStart

    Regards,

    Wesley

  • yes! that works! thanks Wesley, and could you tell me if there is any settings to reduce the power consumption? I've changed the frame periodicity to 1000("frameCfg 0 0 1 0 1000 1 0"), is there any other configuration I can set?
  • Hi Leon,

    You can try Low power ADC mode, LDO bypass mode, and here's a ti-design you can refer:
    www.ti.com/.../TIDEP-0091

    Regards,
    Wesley
  • ok, thanks!