This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1443BOOST: AWR1443BOOST: TX output power reduction

Part Number: AWR1443BOOST
Other Parts Discussed in Thread: MMWAVE-SDK

Hello,

regarding to this Thread, the TX power can be reduced using the profilecfg command of the the mmwave Sensor.

Hower, when settting any of the mentioned valid values the selected signal level is still on the same level as without the recution.

I tested the setting in scattering mode and with the Heatmap using SDK Version 1.0 and 1.1 with 1443 and 1463 Boost kit.

How could i observ the reduction in other ways then comparing the signal level?

Best regards

Jon