This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDC1000-TDC7200EVM: Driver problem

Part Number: TDC1000-TDC7200EVM

I am using windows 8.1, I did those steps in the manual :

"If you do not see TDC1000_7200_EVM and instead see MSP430-USB Example, complete the following
steps:
1. Open the Device Manager and find the MSP430-USB Example device.
2. Right-click and choose Update Driver Software.
3. Select Browse my Computer for driver installation. Navigate and select the folder containing the
TDC1000_7200_EVM_DRIVER.inf file.
4. Close the setup window when the installation is complete. The Device Manager should now display
TDC1000_7200_EVM followed by a COM port number. Take note of this number as it will be required
to connect to the board from the GUI."

But I received the message "
windows can not find the driver software for the device"

Please, could you send me the file TDC1000_7200_EVM_DRIVER.inf ?

Do you have a suggestion about this problem?

Best regards