Other Parts Discussed in Thread: TDC1000
I am using windows 8.1, I did those steps in the manual :
"If you do not see TDC1000_7200_EVM and instead see MSP430-USB Example, complete the following
steps:
1. Open the Device Manager and find the MSP430-USB Example device.
2. Right-click and choose Update Driver Software.
3. Select Browse my Computer for driver installation. Navigate and select the folder containing the
TDC1000_7200_EVM_DRIVER.inf file.
4. Close the setup window when the installation is complete. The Device Manager should now display
TDC1000_7200_EVM followed by a COM port number. Take note of this number as it will be required
to connect to the board from the GUI."
But I received the message "
windows can not find the driver software for the device"
Please, could you send me the file TDC1000_7200_EVM_DRIVER.inf ?
Do you have a suggestion about this problem?
Best regards