This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1642: Is there any way to reduce the power consumption?

Part Number: IWR1642
Other Parts Discussed in Thread: TIDEP-0091, IWR1443BOOST, IWR1443,

Based on this thread, I was wondering if any of this would apply to the IWR1642?

"There are two current fixes to reduce the power, replacing C22 on the EVM with a .022uF cap, and the IWR1443 ES3 40Mhz QSPI load, the combination of these two reduces the 140ms boot time to 27ms."

Would either of these be applicable to the current Rev-A EVM boards/ES1.0 devices?

Thanks,

Aaron