Hi,
I have a questions, In the CLI config command. The unit for the frame trigger delay field in frameCfg is ms. So I tried to set this value to 1ms, but I got a error code reads as "RL_RET_CODE_FRAME_TRIG_DELAY_INVAL_IN". The comments of this error code indicates that "Frame Trigger delay > 100us". Does that means the maximum delay is 0.1ms? Is it possible to delay several milliseconds?