Part Number: TDC1000-TDC7200EVM
Hello, I am using TDC1000-TDC7200 EVM development board for water level sensing, currently, I am testing it with an acrylic container with a height of approximately 12cm and width of 6cm. For which I am using a 1MHz transducer and it works perfectly. Now, I need this to sense the water level of a tank of approximately 2-meter height and width of 1 meter. So, how should I choose my transducer and what frequency should it be so that measurements can be accurate? I have gone through the application notes but still cannot figure. Would someone help me!