Dear, All
The customer has a question about the pattern coil used for the LDC1312.
They use two LDC1312 and use four pattern coils side by side.
Measurement is carried out using two coils at the same time, but it is always considered not to use adjacent coils at the same time.
The diameter of the coil is assumed to be 8 mm. In this case, how much should the distance between the coils be so that adjacent coils do not influence the measurement?
Please tell me if you have recommendations.
Also, please tell us the possibility of how the adjacent coils created will affect.
Thanks, Masami M.