Other Parts Discussed in Thread: AWR1243, AWR1642
Hi,
I am using AWR1243+TSW1400 and Radar Studio to capture ADC data. I am able to capture the data in my PC. The post processing of Radar Studio also works fine.
The data is test data generated with an object at (4,3) m moving at (0.1,0.1)m/s. This was generated through the Test Source tab in Radar Studio. The post processing of radar studio successfully detects the object.
The RS screenshots are as below,
The Matlab code that i am using is:
The range plot is,
As you can see, the Range plot is entirely different that the Actual from Post_proc tab.
I would like to point out that the matlab code here works correctly with ADC capture data of AWR1642. Hence I suspect the Radar Studio writes the bin file in a different format than ADC data capture.
I suspect I am reading the data somehow wrongly form the way that it is written by Radar Studio. Can anyone help me on how to read the data properly in Maltab.
Thanks in Advance,
Santhana Raj