Hello-
We are using the AMC6821 to drive a Delta PFC0612DE-F00 fan at 12V at about 1.5A. The fan is driven directly with a pull up to 3.3V on PWM_OUT. Occasionally the AMC6821 will get hot (60-70 degrees C), even at room temperature, and the fan speed will go to maximum.
Is it OK to drive the fan directly, without an intervening FET? What are the voltage and current rating on the PWM_OUT? Thanks and Best Regards,
-Tim Starr on behalf of MP@SB