This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1443BOOST: Demo not connecting to Demo Visualizer

Part Number: IWR1443BOOST
Other Parts Discussed in Thread: IWR1443

Hi, 

I installed the High Accuracy project and was using the visualizer for a while. It now does not connect to the demo, I can Load and send config still, the hardware says connected but there is no data being displayed. Is there a way to monitor the output of the comm port or know if there is data being streamed out of the device?

Thanks

Garrett

  • Garrett,

    After you send config by visualizer, you can close the visualizer and open a common serial port terminal to connect to XDS110 class auxiliary data port. If there is data output from IWR1443 uart port, you should see data on the serial port terminal. Be noted if the baud rate of serial terminal is not set to 921600, you may see messy code on terminal. You can also use oscilloscope to detect the IWR1443 related uart pin to check if there is data output.