This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1642BOOST: DMM-interface

Part Number: AWR1642BOOST
Other Parts Discussed in Thread: AWR1642

Hi,

I work with the AWR1642Boost for a while. Now, I want to use the DMM-interface.

The goal is to feed radar data into the AWR1642. This data shall be analyzed by the AWR1642 and sending back the detected objects and the velocity over the UART interface.

After a look into the technical reference, I’m not sure about which data are await at the data pins. If I use e.g. 4 data pins, act it like 4 RX antennas and each pin awaits the data of a single RX antenna?

A short example of which data need to be send to which pin to have a “playback” would be very helpful.

Is there an example script how to configure the dmm-interface for Matlab?

And how to feed the pins? Using a function generator?

Thanks,

Marius