Hi,
I'm having troubles with the output value variation regarding the increase of the distance.
This means that the value I get when the sensor is very close to the target versus the value I get when the target is not that close, keep constant whatever value of the IDRIVE.
This range I obtain corresponds always to a variation of 10uH, independently to the value selected for IDRIVE on each channel (I use four sensors). However, when I use the EVM, if I change the IDRIVE through your application, the span of increases.
I have set the RP_OVERRIDE_EN, the SENSOR_ACTIVATE_SEL and the AUTO_AMP_DIS to '1'
I guess that perhaps I have left any "enabling" option disabled, but I don't find any on the datasheet.
Any light on this?
Thanks in advance,