This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDC7200: Controlling multiple TDC7200

Part Number: TDC7200


Hi,

I would like to place multiple TDC7200 chips using one controller.

1. SPI

I think it is fine to connect SCLK/SDIN/DOUT to each bus routed to the controller, and give multiplexed CSB signals. Just would like to double check this!

2. ENABLE/INTB/TRIGGER

Can I also tie INTB/TRIGGER signals from different TDC7200 to each bus, if I give different ENABLE signals to each chip and enable only one of them? In other words, if the chip is not enabled, are INTB and TRIGGER at the high-impedance state?

Thank you!