Hi,
I am working with the doppler-range-heatmap and I am wondering about the levels (colors).
In the range profile for zero velocity (doppler = 0) the power levels are given in dB. In the heatmap instead we get levels like 4000, 5000 and so on.
How is the relation between the range profile power levels and the doppler-range-heatmap power levels?
I would also have this question for the variable "peakVal" in the javascript code of the mmWave DemoVisualizer.
Could you explain these relationships?
Thank you,
Alessandro
P.S.: Actually I'm using firmware version: mmWave SDK 1.1.0.2.