Part Number: LM63
Tool/software: Linux
HI,
Our customers have LM63 on custom board with i.MX6.
They say they have incorporated the Linux driver in the next web, but they do not display the parts related to FAN.
http://www.ti.com/tool/lm63sw-linux
root@imx6qpdlsolox:~# ls /sys/bus/i2c/drivers/lm63/0-004c/hwmon/hwmon0/ alarms pwm1_auto_point4_temp temp1_input device pwm1_auto_point4_temp_hyst temp1_max name pwm1_auto_point5_pwm temp1_max_alarm of_node pwm1_auto_point5_temp temp2_crit power pwm1_auto_point5_temp_hyst temp2_crit_alarm pwm1 pwm1_auto_point6_pwm temp2_crit_hyst pwm1_auto_point1_pwm pwm1_auto_point6_temp temp2_fault pwm1_auto_point1_temp pwm1_auto_point6_temp_hyst temp2_input pwm1_auto_point1_temp_hyst pwm1_auto_point7_pwm temp2_max pwm1_auto_point2_pwm pwm1_auto_point7_temp temp2_max_alarm pwm1_auto_point2_temp pwm1_auto_point7_temp_hyst temp2_min pwm1_auto_point2_temp_hyst pwm1_auto_point8_pwm temp2_min_alarm pwm1_auto_point3_pwm pwm1_auto_point8_temp temp2_offset pwm1_auto_point3_temp pwm1_auto_point8_temp_hyst uevent pwm1_auto_point3_temp_hyst pwm1_enable update_interval pwm1_auto_point4_pwm subsystem
What kind of points should be checked so that parts related to FAN can be used?
This is the case when the DTS file is as follows.
lm63: lm63@4c {
compatible = "national,lm63";
reg = <0x4c>;
};
Best Regards,
Kouji Nishigata