This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1642BOOST: IWR1642BOOST pplcount application custom gui

Part Number: IWR1642BOOST


Hi all,

I started evaluating the IWR1642BOOST kit with the pplcount application.
There is the same GUI compiled for example with visual c or c#  environment?
Is there an example of a GUI interface developed without Matlab?
I'm trying to know what could be the easiest way to create a gui untying from Matlab.
I have to develop an application to evaluate obstacles under a certain distance (0,5m ... 6m).

What can be the starting example project to fit it?

Thanks

  • Hello Giorgio,

    The structure of the UART data stream is documented in the below file, in the Data Formats section towards the end.

    C:\ti\mmwave_industrial_toolbox_2_3_1\labs\lab0011-pplcount\docs\pplcount_user_guide.html

    You may also be interested in the customization guide just after the Data Formats section that describes the compile-time customization capabilities of our firmware.


    Best regards,
    François.