This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LDC1101: No unread LHR conversion data is available.

Part Number: LDC1101


Howdy,

I am using 3 LDC1101 inductance-to-digital converters. I'm configuring the registers of all 3 sensors in the exact same manner. The relevant register settings are given below:

Field

Field Setting

Field Value

Register

Addr

Value

Binary

Hex

Binary

Hex

Decimal

HIGH_Q_SENSOR

Enabled

b1

RP_SET

b0000'0001

0x01

b10100101

A5

165

RP_MAX

24kOhm

b010

RESERVED

0

b0

RP_MIN

3kOhm

b101

C1

6 pF

b11

TC1

b0000'0010

0x02

b11011110

DE

222

R1

33.9 kOhm

b11110

C2

24 pF

b11

TC2

b0000'0011

0x03

b11111111

FF

255

R2

68.6 kOhm

b111111

MIN_FREQ

14

b1110

DIG_CONF

b0000'0100

0x04

b11100111

E7

231

Reserved

0

b0

RESP_TIME

6144

b111

RESERVED

0

b000000

ALT_CONFIG

b0000'0101

0x05

b00000001

0x01

1

SHUTDON_EN

Disabled

b0

LOPTIMAL

LHR

b1

INTB2SDO

Enabled

B1

INTB_MODE

1010

0x0A

B10100000

0xA0

160

RESERVED

0

b0

INTB_FUNC

LHR DRDY

B100000

RESERVED

0

b000000

START_CONFIG

b00001011

0x0B

 

 

 

FUNC_MODE

Sleep

b01

b00000001

0x01

1

Active Conversion

b00

b00000000

0x00

0

RESERVED

0

b0000000

D_CONFIG

b00001100

0x0C

b00000001

0x01

1

DOK_REPORT

Disable amplitude regulation

b1

RCOUNT[7:0]

750

b11101110

LHR_RCOUNT_LSB

b00110000

0x30

b11101110

238

0xEE

RCOUNT[15:8]

b000000101

LHR_RCOUNT_MSB

b00110001

0x31

b00000010

2

0x02

RESERVED

0

b000000

LHR_CONFIG

b00110100

0x34

b00000010

0x02

2

SENSOR_DIV

4

b10

However, I am only able to read LHR count from one of the sensors. If I read the LHR_STATUS register of the other two sensors the value is 0x01 meaning no error but also no unread LHR conversion data is available. Why would one sensor continuously convert and report DRDY on the SDO pin and the other two LDC1101's not? 

I'd appreciate any information that you have to offer.

Thank you,

Alex M.