Tool/software: Linux
Hello,
I am playing and trying AWR1443BOOST to see if we can use the radar sensor in our drone application. Every time I change the configuration, I need to reset the EVM to make the changes "being effect". I believe there will be an API to write the GPIO pin of "reset", would you mind guide me on how to do this.
I have this question, as we want to switch between resolution and range: high resolution (4cm) with range of 4.5m, vs., normal resolution (30cm) with range of 16m. That means when the object is far, normal resolution with long range; while the object is close, high resolution with short range.
I would like your confirmation that we can do the switch between high resolution and normal resolution online. If the change of this configuration requires reset to take effect, is there an online reset function, and if there is such reset function, how long will it take into effect.
Thanks!
Best Regards,
Tao Wang
Automodality Inc.