Hi,
I am testing out both the 1443 and the 1642 using the High Accuracy Demo lab. They both seem to have an offset. I take measurements spaced 0.1 inches apart over 2 inches, 20 locations, and average approximate 75-100 samples for each location. The results show the radar thinks that the target moves closer to 0.075 inches farther each time. When this is all added up there is a significant error comparing the first and last measurement. Has this been observed before and is there something that I should take into account to fix this problem?
Thanks
Garrett