Hi,
Using the following, I have made a program to bring LEDs together,
if there are people moving within a certain range.
mmwave_industrial_toolbox_2_2_0
lab0011-pplcount
mmwave_sdk_01_01_00_02
BORD:IWR1642BOOT
At this time, I would like to do the following, is it possible?
・ I want to display suspended objects (wooden walls) on a Point Cloud together with moving people.
I already tried the following method, but there were no walls, people, things stopped on the screen of pplcount_gui.exe.
[1].With mmw Demo Visializer, disable "clutterRemoval" "peakGrouping",I Create a cfg file.
[2].Apply the created cfg file to pplcount_gui.exe.
Some parameters have been modified according to lab0011 - pplcount default file.
(adcbufCfg,profileCfg,frameCfg,cfarCfg,doaCfg,trackingCfg)
[3].There are many points on the screen, but unlike the mmw Demo Visializer, there are no ones that are stopped.
[4].I already referred to the following.
-IWR1443BOOST: Detecting Wall Profiles
e2e.ti.com/.../678983
-IWR1642BOOST: Detection of a wall
e2e.ti.com/.../633326
TI Resource Explorer の中のVery Fine Motion Detection Experiment
dev.ti.com/.../
mmwave_sdk_user_guide.pdf(Version 1.1)